Recently searched
    /
    Microscopes – A Complete Guide
     
      • Published Mar 7, 2023
      • Last Modified Aug 29, 2023
    • 7 min

    Microscopes – A Complete Guide

    What are microscopes, what are their uses, and what types are available? Discover more in our complete guide.

    This complete buyers’ guide to microscopes includes a detailed look into the various models that are available, explaining their key features and how microscopes are typically used on a day-to-day basis.

    What are Microscopes?

    Microscopes are familiar instruments, commonly found in laboratories around the world. They are used to magnify and examine objects and details which are often too small to see with the naked eye.

    How Do Microscopes Work?

    Microscopes use varying methods to magnify small objects and details, usually for scientific or industrial purposes.

    The most widely used design is the optical microscope which directs light through a carefully calibrated combination of lenses with varying focal lengths. These curved pieces of glass or plastic then bend that light, spreading out the rays emitted by tiny objects under examination in order to generate a magnified image.

    However, this is just one example and other types of microscope use entirely different methods to produce much more powerful magnification. We will cover some of the additional microscope types in the following section.

    What are the Different Types of Microscope?

    There are four principal types of microscope. These are:

    Optical/Compound Microscopes

    Main Benefits :

    • The most common type of microscope
    • Features eyepieces to view imagery

    Ideal Applications :

    • Microelectronics, biotechnology, microbiology, education

    Stereo Microscopes

    Main Benefits :

    • Two eyepieces as standard
    • 3D viewing

    Ideal Applications :

    • Studying solid objects, close work such as surgery or dissection, botany, working with electronics

    USB Microscopes

    Main Benefits :

    • Portable plug-and-play functionality
    • Imagery displayed on a PC screen

    Ideal Applications :

    • Examining flat objects and printed circuit boards, scientific research requiring the observation of moving objects such as microorganisms

    Electron Microscopes

    Main Benefits :

    • High magnification and resolution
    • Exceptional quality imagery

    Ideal Applications :

    • Scientific applications, studying biological and inorganic objects, industrial purposes including failure analysis and quality control

    Let’s take a look at each type in more detail.

    Compound Microscopes

    The optical microscopes familiar from education and scientific laboratories are technically known as compound microscopes. This is because they combine two or more lenses to generate a magnified image. This distinguishes compound microscopes from simpler, single-lens microscopes – a category which includes magnifiers.

    The main lenses within a compound microscope are:

    • Objective Lens – directly above the glass slide on which the object under examination will be placed
    • Ocular Lens – this is more commonly known as the eyepiece

    These are both convex lenses, meaning that they curve outwards. In more complex models, both the objective and the ocular lens may consist of multiple lenses linked together.

    How Does a Compound Microscope Work?

    The short focal length objective lens focuses an image of the object under examination onto the upper ocular lens, which has a longer focal length.

    Stereo Microscopes

    Stereo microscopes essentially combine two separate microscopes into one. This means that the instruments have two optical paths, each with their own objective and ocular lens.

    The result is that slightly different viewing angles are produced for each eye, thereby generating a 3D image of the object under examination. These instruments are also known as dissecting microscopes.

    USB Microscopes

    USB microscopes are powered by everyday USB ports. Instead of an eyepiece, USB microscopes display the magnified image onto a PC screen.

    Some USB microscopes can be used with bespoke software, allowing greater flexibility and manipulation of the object being examined.

    See for Yourself!

    Take a look at our video to see the key features of the RS Pro Wi-Fi microscope and how it works.

    These handheld digital microscopes feature built-in Wi-Fi transmission, enabling a seamless transition from instrument to screen. Wi-Fi microscopes offer a high degree of flexibility and greater functionality compared to alternative types, allowing the user to measure, copy, and transfer both images and video in real-time.

    Electron Microscopes

    Electron microscopes make use of an accelerated beam of electrons to generate an image of the object under examination. The image is produced as each electron bounces back onto the device’s specialist lens. Since they do not rely on conventional lenses, electron microscopes can produce images with significantly greater magnification and resolution.

    Electron microscopes are typically powerful, high-end devices primarily used in scientific settings. There are two key types – SEM (scanning electron) and TEM (transmission electron). The former produces a 3D image and the latter produces a 2D image.

    X-ray microscopes also work on a similar principle, using electromagnetic radiation to produce magnified images.

    Popular Microscope Brands

    Below are just a few examples of popular microscope brands. Each offers high-quality, specialist instruments ideal for a wide range of magnification purposes and applications.

    Where are Microscopes Used?

    Microscopes are widely used in laboratories and similar environments by professionals in a variety of scientific fields, including:

    • Geology
    • Biology
    • Botany
    • Medicine
    • Forensics
    • Chemistry

    Microscopes are also used in industry – for example, pharmaceutical manufacturing and engineering. In addition, they are a common inclusion in education environments including school and university laboratories.

    In each case, microscopes are used to examine fine details invisible to the naked eye or objects too small to be seen otherwise. This could include microscopic organisms, plant and animal cells, and chemical structures, to name just a few examples.

    To cater to such a wide range of applications, microscopes are produced in different shapes and sizes, ranging from larger designs to light, portable handheld models.

    How Much Magnification Do Microscopes Provide?

    The magnification strength of a microscope varies between different models. Standard compound microscopes typically magnify objects by either 10, 20, 40, 100, or 400 times, but industrial models can generate images which have been magnified over 1,000 times. Some electron microscopes can take that even further, providing up to as much as 10 million times magnification.

    FAQs

    What Microscope is Used to View Bacteria?

    In most cases, a reasonably powerful compound microscope will provide sufficient imagery of bacteria and similar microscopic organisms.

    What Microscope is Used to See Nanoparticles?

    Microscopic particles measuring between one and one-hundred nanometres are referred to as nanoparticles. A nanometre is hard to imagine – just one billionth of a metre. As a result, an electron microscope is needed to view such small particles. Either a SEM or a TEM model can deliver sufficient power for this purpose.

    What Year was the Microscope Invented?

    Lenses as we know them today date back as far as the 13th-Century when eyeglasses were first devised. The earliest compound microscopes appeared in Europe circa-1620.

    The identity of the microscope’s original inventor is not known for certain. However, two of the likeliest candidates are Dutch spectacle-maker Zacharias Janssen and Hans Lippershey, Janssen’s neighbour and rival spectacle-maker. Hans patented an early telescope design in 1608. An alternative theory suggests that astronomical pioneer Galileo Galilei invented the microscope by changing the focus of his telescope.

    Which Microscope is the Most Powerful?

    The most powerful microscope in the world is the TEAM 0.5 at the Lawrence Berkeley National Laboratory in California. This transmission electron microscope boasts a magnification power of one ten-millionth of a millimetre – less than half the width of a single hydrogen atom!

    How Do I Choose the Right Microscope?

    The best microscope will ultimately depend on your requirements and the specifics of your project or environment. Standard compound microscopes are generally fine for most everyday magnification needs, yet more advanced, industrial models are available for those who need the extra magnification that a powerful electron microscope can provide.

    It is also important to choose the right microscope accessories to complement your instrument. From additional eyepieces to handy desktop stands, bases and replacement lamps, accessories can be used with a wide range of microscope models to ensure that instruments are functioning to their maximum capacity.