Press Releases
SmartEverything development board for the Internet of Things now available from RS Components
New IoT development board from Arrow Electronics offers a wide range of sensors and communication interfaces including access to the wide-range SIGFOX communications network
Taiwan, 6 January 2016:
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has announced availability of the SmartEverything Internet of Things (IoT) development kit from Arrow Electronics. The new SmartEverything ‘Fox’ board is an Arduino-form-factor IoT system-on-module that comes with a multitude of factory-bundled I/O ports and sensors and with a highly energy-efficient wireless connectivity technology.
Key elements of the SmartEverything system board are the Atmel D21 ultra-low-power MCU, based on the 32-bit ARM® Cortex®-M0+ processor, and a SIGFOX communications module for IoT connectivity. The SIGFOX standard is energy efficient and wide-transmission-range technology that uses UNB (Ultra Narrow Band) based radio technology and offers low data-transfer speeds of 10 to 1000 bits per second. However, very importantly, it is highly energy efficient and typically consumes only 50μW compared to 5000μW for cellular communication for example, meaning significantly enhanced battery life for mobile or portable IoT devices.
The SIGFOX connectivity is powered by the Telit LE51-868S high-performance module that is a certified SIGFOX gateway and covers the 863-870MHz unlicensed ISM band. It is preloaded with the SIGFOX network protocol stack and the Telit proprietary Star Network protocol. In addition, the Telit cloud management software enables easy connection up to the cloud.
The SmartEverything board also includes an Atmel Crypto Authentication chipset; an 868MHz antenna; a GPS module with embedded antenna for localisation applications, which supports the GPS, QZSS, and GLONASS standards, as well as being Galileo ready; a proximity and ambient-light sensor; a capacitive digital sensor for humidity and temperature measurement; a nine-axis 3D accelerometer, 3D gyroscope and 3D magnetometer combination sensor; a MEMS-based pressure sensor; an NTAG I2C NFC (Near Field Communication) module; and a Bluetooth Low Energy (BLE) transceiver module.
The SmartEverything PCB measures only 68.8mm x 53.3mm with the USB connectors, power jack and antenna extending beyond the board. The board can be powered in three ways, via: two AA 1.5V batteries (1.4V to 3.2V); a 5 to 45V external power supply; or the 5V mini-USB connector. Enabling fast and easy software development, the SmartEverything Fox board is supported by the Arduino IDE and Atmel Studio IDE (Integrated Development Environment).
The SmartEverything SIGFOX board development kit is now shipping from RS at a cost of £77.99. More information on the RS range of products for the Internet of Things is available at /web/generalDisplay.html?id=i/iot-internet-of-things.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping around 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2015 had revenues of £1.27bn.
For more information, please visit the website at www.rs-online.com.
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com