Press Releases
New Compact Arduino Mini Wireless Development Board Now Available From RS Components
Arduino Yun Mini provides an affordable, small and lightweight Linux-based WiFi prototyping solution
Taiwan, 14 July 2015:
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has announced that it is extending its Arduino portfolio of open-source electronics development and prototyping boards with the addition of the new Arduino Yun Mini.
Aimed at embedded engineers, hackers and students, the Arduino Yun Mini is a redesign of the Arduino Yun WiFi microcontroller board and has been re-engineered to be used with a breadboard, making prototyping easier, and also provides its functionality in a light and highly compact package.
The Yun Mini has approximate PCB dimensions of 71.1mm x 22.9mm, which is less than half the area of the Arduino Yun PCB, which has dimensions of approximately 68.6mm x 53.3mm with its USB connector extending the length to approximately 73mm. In addition, the weight of the Yun Mini at 16g is half that of the Yun. The board's small size makes it ideal for use in small spaces and especially projects for home automation, where locating smaller devices in small boxes can improve siting flexibility.
The Yun Mini offers an affordable breadboard PCB with an ATmega32u4 microcontroller and the Qualcomm Atheros AR9331 system-on-chip IC with a MIPS 24K CPU, which operates at up to 400MHz and supports a Linux distribution based on OpenWRT called Linino. A bridge library enables communication between the two processors, providing Arduino programs the ability to run shell scripts, communicate with network interfaces and receive information from the AR9331 processor.
The board has built-in WiFi (IEEE 802.11b/g/n operation up to 150Mbps) and supports 20 digital input/output pins, seven of which can be used as PWM outputs and 12 as analogue inputs. Other specifications include a 16MHz crystal oscillator, a micro-USB connector, an ICSP header, two reset buttons and one user button.
The Yun Mini is similar to the Arduino Leonardo in that the ATmega32u4 has built-in USB communication, eliminating the need for a secondary processor, which allows the Yun Mini to appear to a connected computer as a mouse and keyboard, as well as a virtual (CDC) serial/COM port.
The Yun Mini can be customised from a choice of up to two out of three available accessories, which are the dogRJ45, the dogUSB and the dogUSB eMMC. The dogRJ45 is a 10/100Mbps Ethernet port; the dogUSB is a USB A type connector with USB 2.0 hub that features a slot for a mini SD to extend the memory of the board; and the dogUSB eMMC is a USB port type A with an integrated 4GB of Flash.
The board can be powered via the micro-USB connection with 5V DC, which is the recommended option. However, a regulated 5V DC can also be used to power the board via the Vin pin. The Yun Mini can be programmed with Arduino software downloaded fromarduino.org/downloads or the Linino IO from www.linino.org.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping around 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2015 had revenues of £1.27bn.
For more information, please visit the website at www.rs-online.com.
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com