Press Releases


RS Components extends rapid-prototyping product portfolio with pair of high-quality 3D printers from Zortrax

Professional 3D printers and accessories provide the ideal prototyping equipment for design engineers, enabling faster time to market

Taiwan, 30 June 2017:

RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, is extending its portfolio of high-quality 3D printers with two new high-reliability printers from Zortrax for a wide range of professional users. The printers provide design engineers with the ability to produce detailed, accurate and cost-effective rapid prototyping of their designs, enabling a shorter development process and quicker time to market. Engineers can quickly produce concept mock-ups, prototype products for functional testing or even low-volume production for a wide variety of applications across many industries such as automotive, industrial or robotics.

Employing single-extruder LPD (layer plastic deposition) printing technology, the reasonably priced Zortrax M200 and M300 3D printers are reliable, efficient and offer exceptional quality with high dimensional accuracy and repeatable precision. This enables the high-quality printing of detailed elements that duplicate models without any loss of the original appearance, as well as completing extensive print jobs with almost no maintenance.

The M200 pack is a fully integrated plug-and-play system that allows users to get up-and-running immediately and includes the 3D printer, starter kit, dedicated intuitive software bundle Z-SUITE, and compatible material. Specifications of the M200 include: workspace dimensions of 200 x 200 x 180mm; 90 to 400-micron resolution, wall thickness capability of 400 microns (minimum) to 800 microns (optimum); and single printable point resolution of 400 microns. Other key specifications include material diameter of 1.75mm and a nozzle diameter of 0.4mm.

Physical dimensions of the printer are 345 x 360 x 430mm without the material spool and 345 x 430 x 430mm with the spool. In addition, there are a number of extra options available including the Hotend V2, perforated plate V2, and side covers, which keep a stable model temperature during the printing and cooling process to reduce the risk of warps and cracks.

Materials are available in a wide selection of professional grades, qualities and colours to suit different design requirements, and include Z-ABS, Z-ULTRAT, Z-HIPS, and Z-PCABS. The Z-ULTRAT filament comes in pastel shades of yellow, pink, purple, blue and turquoise; Z-ABS in white and pure black; Z-PCABS is a polycarbonate ABS ivory filament; and Z-HIPS comes in black. The range also enables the selection of materials that offer high durability against mechanical stress or high resistance to temperatures or even chemicals.

The Zortrax M300 3D printer builds upon the capabilities of the M200 and offers a larger workspace with dimensions of 300 x 300 x 300mm and 140 to 300-micron resolution, optimal wall thickness dimension of 800 microns, and single printable point resolution of 400 microns. The M300 is ideal for designs using the Z-HIPS material, and provides a spool preview to allow users to check the material usage and colour. The M300 pack comprises the printer, side covers, starter kit, key to Z-SUITE software, and two spools of material.

Compatible with stl, obj, dxf and 3mf file types, both machines support Mac OS X/Windows 7 and newer versions, and have access to a helpful model library. Further accessories available for both machines include the Zortrax 40 x 40mm fan cooler and extruder cable with adaptor.

The Zortrax M200 and M300 3D printers are shipping now from RS across EMEA and Asia Pacific. This new range strengthens the existing comprehensive selection of 3D printers and accessories stocked by RS: /web/generalDisplay.html?id=i/3d-printing.

About RS Components

RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping around 50,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2017 had revenues of £1.51bn.

For more information, please visit the website at www.rs-online.com.

Further information is available via these links:

Twitter: @RSElectronics; @alliedelec; @designsparkRS

RS Components on Linkedin
http://www.linkedin.com/company/rs-components

RS WeChat ID: RS_Components_CN

Relevant Links:

Electrocomponents plc
www.electrocomponents.com

RS Components
www.rs-online.com

DesignSpark
http://www.designspark.com