Press Releases
Touch, Discover, Solve with new Keysight InfiniiVision 3000T X-Series oscilloscopes from RS Components
Intuitive user interface and powerful analysis tools enable fast and confident troubleshooting
Taipei, Taiwan, 26 March 2015:
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, has added the powerful new Keysight InfiniiVision 3000T X-Series oscilloscopes to its extensive test and measurement portfolio featuring the industry’s leading brands.
The 3000T X-Series is featured for easy, intuitive operation. An 8.5-inch capacitive touchscreen with gesture support helps quickly configure oscilloscope functions, simplifying complex tasks such as setting triggers. Conventional buttons and knobs also provide access to the intuitive controls.
The oscilloscopes allow a straightforward Touch, Discover, Solve approach. Discovery is aided by features such as the very high uncompromised update rate of up to one million waveforms per second, combined with zone touch triggering for isolating any complex signal in seconds. Segmented smart memory allows users to capture long time periods at high sample rates, and dedicated search tools help navigate deep memory.
Solve tools include protocol analysis, integrated 20MHz arbitrary-waveform generator and 3-digit DVM. Further options include an 8-digit frequency counter/totaliser, Mixed-Signal Oscilloscope (MSO) channels, hardware-accelerated mask/limit testing, power measurement and analysis, and a power-rail probe for making power integrity measurements. Rich mathematical functions include gated FFT. Keysight’s BenchVue next-generation remote connectivity and Infiniium Offline scope data analysis tool are also available.
Standard models have bandwidths from 100MHz up to 500MHz, with two or four digital-storage (DSO) channels plus 16 optional MSO channels. Upgrade packs allow users to add extra features and measurement applications.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer around 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping more than 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include semiconductors, interconnect, passives and electromechanical, automation and control, electrical, test and measurement, tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2014 had revenues of £1.27bn.
For more information, please visit the website at //www.rs-online.com
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com